Part Number: PTN78060W Dear colleague,
Our customer wants to know the control chip part # in PTN78060W.
So could you please show it?
Thanks a lot!
Best Regards,
Rock Su
Part Number: PTN78060W Hello experts,
My customer considers to use PTN78060W.
To check whether PTN78060W can be used in their system, other thermal information (e.g. RθJA, ψJT) is needed.
On datasheet, there is only Ta information.
Do you have…
Part Number: PTN78060W Hi
I am planning to use PTN78060W in one of our boards. The board would be powered from either 24VDC or 5VDC. So it has 3Way Power connector (terminal block)
For 24VDC Vin case
the positive of 24Vin goes straight to Vin Pin…
Hi,
I recently purchased the PTN78060WAZT, and I am wondering if the development board has built in Cin, Cout and Rset?
If not, Can I use a 2.2uF ceramic cap with 100V rating, and 100uF ceramic for the Cout?
Thanks,
Hoa
Other Parts Discussed in Thread: PTN78060W Hello,
Regarding to the subject above, I'm wondering if we're not following its requirements. In my case, I want a Vout = 12V with Vin varies between 12-14V and Rset = 21kohm. Will Vout be maintaining its 12V…
Other Parts Discussed in Thread: PTN78060W I have a PTN78060W on three of 500 boards that 20% of the time it will power on with an output voltage of 3.52Vdc vs. 3.31Vdc. I have attached an excerpt from the schematic. Input voltage to the circuit = 10…
Other Parts Discussed in Thread: PTN78020W Hello,
I'm designing a power supply board that operates in an environment that could potentially reach 60C ambient. Is there a recommended way of dissipating the heat from the module? Heat sink? Thicker Cu…