My customer wants to know if you can set up external components using the inhibit line to stretch the internal soft start when power is applied. The customer wants to reduce the inrush current caused by capacitive loading.
Is it possible to pre-bias…
Other Parts Discussed in Thread: PTN78060W , UCC29002 Hello,
Can I connect two PTN78060w in parallel (two outputs connected together) and doubling the output current capability?
Thanks in Advance.
Giora
Hello Mike,
PTN78060W Product Folder page, including the datasheet, are located here: http://www.ti.com/product/PTN78060W .
Or is it that you are looking for the PTI datasheet?
At your service,
~Leonard
PTN78060W can be considered replacement for the PT78HT205H. It does not have the same form or fit characteristics. PTN78060W has similar electrical characteristics, however it is slightly smaller with 7 power pins and it is rated to 3 amps.
If you have…
Part Number: PTN78060H Other Parts Discussed in Thread: PTN78060W , Hi,
I want to use ptn78060W module.
I read page 6,7,8 and 9 :
"The temperature derating curves represent the conditions at which internal components are at or below the manufacturer's …
Gweltaz
1. What is the Ramp ON module characteristics V/µs ?
PTN78060W Published data is 0. 5V/msec.5V/msec
All published data in Product specification
PTH08T220Wxx published data is 0.5V/msec
…
Hi Tom,
I had a mistake. This is question as PTN78060W.
and i confirm again.
Should I calculate as Vmin = 2.5 at the following condition?
IC : PTN78060W
Vin : 28V
Vout : 5V
Thanks,
Shimizu
Other Parts Discussed in Thread: PTN78060W Hi,
PTN78060WAD occurs problem.
The problem is how to start up strange such as following.
(I can't share actual waveforms because they are confidential)
This work is problem for my customer set.
Suffix No…
Other Parts Discussed in Thread: TPS65100 , PTN78060W , TPS65100EVM-030 I am having issues with the TPS65100 during startup. We have built a couple 100 modules with no problems. I am searching the components to see if we have a bad part. When operating,…