Hey Lei,
Was this issue resolved? I will go ahead and mark Ron's response as "TI Thinks Resolved."
If the issue was not resolved, please let us know how we may further assist.
All the best, Carolina
Part Number: RC4558 Other Parts Discussed in Thread: LM358B , TL072H , TL082H , LM358LV The customer is using RC4558IDR. they want to figure out that when Vcc- is GND, is the minimum voltage at Vcc+=5V?
or the minimum voltage should be 10V =(+5V - (-5V)…
Part Number: RC4558
Could you offer the R θJC and Tc (Max) ?
In the d/s, there are only T A 、T J 、R θJA, they are not enough for thermal calculation.
Regards
Brian W
Part Number: RC4558 Input offset voltage is TYP 0.5mV, MAX 6mV at 25 ℃. What is the distribution from TYP to MAX? Also, in the full range, only MAX 7.5mV is shown. What is the distribution in the full range?
Part Number: RC4558 Hi,
Greetings for the Day!
I am not able to not the output current limit of this part inside the datasheet.
Can anyone please provide this information?
Thanks
HHS
Part Number: RC4558 Other Parts Discussed in Thread: TL074 , TL084 , LM358 , Hi, I'm a hobbyst and I have purchased : -opamp TL084, TL074, RC4558x2 No one runs, but an LM358 of another manufacturer does the task for this reason I imagine the circuit is OK…
Part Number: RC4558 hello,
1. Could you let me know the SNR parameter of RC4558? Or how to evaluate the SNR performance?
2. For the second SOIC (8), it should be VSSOP. Could help confirm?
Dongbao
Other Parts Discussed in Thread: RC4558 Hello,
We offer the customer the RC4558.
But the characteristic of the Output Voltage Swing is slightly poor against the competitor.
We have a question about the characteristic of the Output Voltage Swing vs Load…