Part Number: RC4580 Hi all
My customer is using the
RC4580 Dual, 32-V, 12-MHz, low noise (6.5-nV/√Hz) operational amplifier RC4580IDR
And they have this question:
The supply is +/-15V, where the -15V is delayed for power on and off vs. the +15V…
Part Number: RC4580 Dears:
when use RC4580 in sensing project, we calibrate it in the product line, but end customer found abnormal accuracy error after several weeks work. Could you please help provide VOS VS time curve to help identify the issue?
End…
Part Number: RC4580 Other Parts Discussed in Thread: OPA2992 , TLV9062 Hi,
One customer downloaded the RC4580 Hspice model, the folder is as following:
He used cadence16.6 SigXplorer PCB SI XL-Analyze-Model Browser-HSPICE Models-rc4580_test.sp ,click…
Part Number: RC4580 Dear Person in Charge,
I'm looking for a graph of the performance of the part in question. List the charts I'm looking for.
・Input resistance ・Relationship graph between power consumption and temperature fluctuation ・Graph of…
Hey Mohit,
We have an encrypted HSPICE model but do not have a simulation model for the RC4580 for TINA-TI or PSpice for TI. There many other automotive audio op amps that do have spice models for your application to verify the application.
https://e2e…
Part Number: RC4580 Hi team, My customer checked XRAY for RC4580IPWR. The lead frame was different depending on the device. Is this a normal product? Sincerely. Kengo.
Part Number: RC4580-Q1 Other Parts Discussed in Thread: OPA1612-Q1 Hi team,
As the title, could you kindly tell me which audio amp can be recommend to customer?
BR
Jiawei
Part Number: RC4580 Hi Team,
Our customer is using RC4580 and noticed that at higher voltage (>3Vrms) the signal experiences amplitude wrapping. Please refer to the schematic diagram test waveform below. Why this occurs and how to eliminate the wrapping…
Part Number: RC4580 Hello Team ,
We are Planing to use RC45 80 for MIC amplifier.
We have two below question :
1. RC45 80 is work as Pre-amplifier or amplifier for MIC Input .
2. If We are using RC45 80 then we can remove MIC BIAS CIRCUT .
3.MIC Input need to…