Part Number: REF200 Other Parts Discussed in Thread: LM234 , LM334 , LM134 Tool/software: Hello TI,
I am planning to build a positive temperature dependence current source for matched JFET pairs, can TI suggest a proper design for the same?
Part Number: REF200 Tool/software: Set REF 2000 to deliver 100uA. a resistance to ground is mounted on the REF200 output. As long as this resistance remains within 10KOHM the current supplied corresponds to 100uA. But if I insert a resistor of 100KOHM…
Part Number: REF200 Tool/software: Hi Team,
I got the part, REF200AU, DC2230+
is this the extended shelf life (ESL) material?
is this still under warranty from TI?
Thanks,
Part Number: REF200 Other Parts Discussed in Thread: LOG200
Tool/software:
Hello, engineers from Texas Instruments, We are planning to test the logarithmic amplifier, but the REF200 we are using cannot simulate the PMT (-100uA-0uA). When it enters the…
Part Number: REF200 Tool/software: Hello,
I am seeing this same issue still.
KNOWNS:
I do not have local admin
admin has to elevate privileges with ThreadLocker
install happens
I get the same kind of pop-up as the previous user saying it can't find…
Part Number: REF200 Tool/software: Hi team,
Could you help if following circuit works OK under 8V supply?
What's the normal voltage work range for the following circuit?
Thanks and Best regards,
Will
Part Number: REF200 Hi team,
I have a customer with the below issue regarding the REF200AU current source. Let me know what you guys think!
"We are using the REF200AU current source and are having some issues with a regulator that feeds it. Under…
Part Number: REF200 Hi,
Would you like to ask, constant current * load resistance < constant current source chip power supply voltage? Or are there any requirements for the load resistance?
Many thanks~
Part Number: REF200 I am considering using REF200 as a current sink (100 uA), but it requires the current sink input voltage is to be a min of 2.5V. I think I have 1.4 V but not 2.5V input.
Can I use the current mirror part of REF200, by grounding pins…