Part Number: REF3112 Other Parts Discussed in Thread: REF31-Q1 Tool/software: Hello Expert,
My customer met a oscillation issue of REF3112. Do you mind helping to have a view on it?
The details are shown in slides.
Best regards,
wenting
Part Number: REF3112 Other Parts Discussed in Thread: REF3012 , REF35 , REF3312 Tool/software: Is spice model available for this part to do LTSPICE simulation?
Part Number: REF3112 Tool/software: Hello E2E Experts,
Good day.
When the IC is sourcing, what is the minimum current it will source and when it is sinking, What is the maximum current?
Regards,
CSC
Part Number: REF31-Q1 Other Parts Discussed in Thread: REF3112 Hello,
on the datasheet there is a remark for the 1.25V variant of the device REF3112AQDBZRQ1
"Minimum supply voltage for the REF3112 is 1.8 V."
Can you please clarify if I can use…
Part Number: REF3112 Hello team,
My customer considers REF3112AQDBZRQ1 instead of REF3112AIDBZT due to delivery reason.
Customer would like to know any differences on the two parts, however all specs including temperature range look same between the two…
Part Number: REF3112 Dear Sir/Ms.
My customer is looking for 1.200 ±5.0mV, 20ppm/°C (SOT23-3 package) for FPGA application. REF3112 can replace others bout different output voltage. I can not find 1.2V output on website. May I have your help to double…
Part Number: REF31-Q1 Tool/software: Hi expert,
1. The application diagram for REF3112-Q1 is as follows.
2. We found that the output voltage has a strong overshoot. on power up, What could be the issue? Are there any methods to optimize this?
looking…
Part Number: REF3112 Hi
My customer use REF3112 at Vin=1.8V of ±3%. So there is a possible Vin_min of REF31112 to be 1.746V. Are there this using method the problem?
Best regards,
Yokota