Part Number: REF3312 We have a question about the output current of REF3312. In the data sheet on page 1, is said that this output current is +-5mA
And on page 5 is said that it is +-30mA
What is the actual value? 30mA or 5mA?
Thanks in advance.
Part Number: REF3312 Hello,
My customer is looking for 1.25V reference having <500us Turn-On Settling Time (to 0.1%) and considering MAX6023EBT12 because it’s Turn-On Settling Time (to 0.1%) is very fast, 30us.
The REF3312 datasheet says Turn…
Part Number: REF3312 Hi Ethan,
You mentioned that total max error is initial accuracy+temp drift(max 30)+line regulation(Max 50)+etc...
Is it correct?
Thanks.
Part Number: REF3312 Hi, From Figure 17, 1 to 10 μF is recommended for CBypass. Is this the recommended value for the effective capacity? If No, how much effective capacitance values do we need? Best Regards, Yuto Sakai
Part Number: REF3312 Hi,
Please tell me the test condition below.
Why is there no current condition in Load regulation condition?
Or what do you mean?
Best Regards,
Yuto Sakai
Part Number: REF3312 Hi,
Could you tell me about Vout accuracy.
When thinking about the worst case of accuracy of Vout taking temperature into consideration,
I understand that it is enough to add "output voltage temperature drift" and "Thermal hysteresis…
Hi Thomas,
Thank you for waiting. The customer took time to respond due to a schematic update.
Closing the device inside a metal enclosure is not an option. The device is battery-powered and tested by applying a constant voltage on a fixed resistor. as…
Part Number: INA129 Other Parts Discussed in Thread: REF3312 , , REF3325 , REF5025 Tenho um circuito que utiliza o Amplificador de Precisão INA129P, quando utilizando o modelo INA129PA, a saída do mesmo apresenta-se próxima da tensão V+. O ganho…
Hi Neguse,
Yes, the REF35125 is currently in preproduction.
If you need it sooner than that, please look at using the REF2025 or REF3312 and follow the same circuit as in the REF35 data sheet.
With a shunt reference, you can use the TLV431B and flip the…
Other Parts Discussed in Thread: REF3312
Hi there,
I am working on a legacy design that uses the REF3312 to supply a 1.25V refererance to a microcontrollers ADC section (Atmel AVR VREF pin) However on one of the ADC channels we now have to work with a…