Hi Zebryk,
That application note is applicable for our entire TI series voltage reference portfolio:
www.ti.com/.../products.html
The smallest series voltage reference is the REF33xx family below I available in QFN. The application note is also applicable…
Amit,
The reference is external REF3330, 3.3V. We test the REF3330 will cause only 1LSB error in full temperature range.
Can you provide any standard test procedue? Or source code to you to check?
Thanks and best regards,
Hardy
Other Parts Discussed in Thread: REF3330 The circuit shown in Figure 1 is a voltage reference with an input over voltage protection. The circuit design and selection of over voltage protection components is optimized for minimum power and maximum input…
Part Number: TMS320F28379D Other Parts Discussed in Thread: THS4551 , REF3330
Hi,
Can you help with my customer's request below:
There is a requirement for simultaneous sampling of 4 currents (4 pole bridge. Can use 12-bit here). Also I have General…
Hi Diego,
Thank you!
Actually, customer need a very low cost reference. Since LP5907 has so large drift as 55ppm, maybe we still need to find a reference. seems REF3030 is the only choice, REF3330 is still high price here.
Do you think so?
Thanks,
Jo…
Other Parts Discussed in Thread: ADS8344 , REF5030 , REF3330 Hello.
I have two design with ADS8344 and the output creates a lot of noise / jumps, app 64 counts.
The other thing is that the output jumps at 16 count and only gives 2, 4, 6 etc in the last digit…
Hi Gary
Device performance specifications are not guaranteed if device absolute maximum specifications are violated. Based on input over voltage level and time duration for which it was appllied there could be partial or complete damage to internal circuit…