Part Number: REF3450 Other Parts Discussed in Thread: LM4120 Dear Specialists,
My customer is considering REF3450T as a substitute for LM4120IM5-5.0/NOPB.
There are some difference between REF3450T and LM4120 and they have questions.
I would be grateful…
Part Number: REF3450 To whom it may concern,
I have a question about REF3450IDBVR.
Is there a possibility of input voltage output as a failure mode?
For example, as below:
- IN=10V. I s there a possibility of OUT_F(OUT_S) = 10V as a failure mode?
…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: REG71055 , REF3450 , REF3430 , TINA-TI I installed software Pspice for TI from TI HP. However their Pspice model can not been found at TI HP.
I hope someone tell me how to fix this problem,
Part Number: REF3450 Hello Team
Q1 About description of "Output short circuit current" in the datasheet, Absolute Maximam ratings says 20mA is maximam, but Electrical Characteristics says 22mA is maximam. What does make this diffelence? and Which value…
Part Number: REF3450 Other Parts Discussed in Thread: REF34-Q1 Pin 1 (NC) of the DBV package is used as " Test pin, connect from 0V to 18V ". We need to use this part in one of our designs as an alternative where we left this pin floating. I've tested…
Part Number: REF3450 Page 3 (table 6.1) of the D/S states under pin 1 (NC): " Test pin, connect from 0V to 18V. " Towards the end of the document is a layout drawing that shows this pin connected. However, this pin is not discussed in the D/S. Can…
Part Number: REF3450
We implemented REF3450 product in our projects.
As per the datasheet ripple voltage of the input should have to filter out at output. But in our project, we are given REF3450 5V regulated output voltage to MEMS accelerometer sensor…
Part Number: REF3450 Hi team,
Could you please share the FMEDA file of REF3450QDBVRQ1 so that my customer can use it to do system level analysis? You can reply to me through emails. Thanks.
Part Number: REF3450 Other Parts Discussed in Thread: TINA-TI , Hi,
I'm struggling to design with the only reference that meets my requirements which is the LT3450. It would be super helpful if you offer this SPICE file unencypted as I'm forced away from…
Part Number: REF3450 Hi Team,
Does turn on time have dependency of temperature? This is because our customer check the Vout turn on time behavior of across temperature. They can see like figure as below. the red line is on datasheet. I add the blue line…