Part Number: REF35 Tool/software: Hello TI team,
We are using some TI ICs in power section of our design. The Designator and its part numbers are as below,
1. U24: REF35300QDBVR
As we have completed the layout we would like to review it from TI team…
Part Number: REF35 Tool/software: hi sir
We would like to design a meter, need a current source to driver the sensor as below
REF35 is a good solution for this application?
thanks
Part Number: REF35 Other Parts Discussed in Thread: OPA388 , , REF102 Tool/software: Hello,
I am trying to build a 500 uA precision current source for a sensor. The circuit should only be powered by a 5 V or 3,3 V power supply and space is very critical…
Hello,
1. ISL60002DIH311Z-TK is a 1.2V voltage reference. The best option is REF35120QDBVR (REF35), which can be pin to pin as shown below:
2. R1243K001A-TR is a buck DC/DC converter. I will allow the buck converter experts comment on the best suggestion…
Part Number: REF35 Tool/software: Hi,
If the VIN voltage falls below VDO + VREF, will VOUT be output? Or will the output stop due to an error?
VDO varies depending on the conditions, but for example, if the current VDO is 0.1V and the REF3525 is used…
Part Number: REF35 Other Parts Discussed in Thread: REF4132 , , REF3425 Tool/software: Hey Team,
My customer is asking if it's okay to short pin NR and VREF together? Will there be any adverse effects?
Part Number: REF35 Other Parts Discussed in Thread: REF70 Tool/software: Hello, My customer is looking for a small size voltage reference device to generate Vo = -1.25V from Vin = 3.3V or -3.3V. Does TI have any solutions to meet their requirements…
Part Number: REF35 Hello,
We are using a REF3525 (2.5V) voltage reference in a design, with an inverting opamp, to generate a -2.5V reference.
Is it possible to wire the device between GND and -5V rails, to generate -2.5V without using an opamp?
Best regards…
Part Number: REF35 Other Parts Discussed in Thread: INA118 , INA826 , , LM2776 , LM2775 , Tool/software: Hey,
we need for a new design a reference voltage with small package. The component should be used as reference voltage for the INA 826 and additional…
Part Number: REF35 We're interested in the very-low power REF35 device with Vout = 1.024V, in the small WCSP (BGA) package. Is this device available (samples/production) ? [Specification provides reference code REF35102YBHR, but also mentions 'please…