Part Number: REF35 Hi Team,
Could you please kindly help to check if we have some automotive REF device which is similar with REF35 and the Iq<3uA could accept by customer.
Relate ref voltage needed by customer including 1.2V, 1.8V,2.2V,2.5V. Thank…
Part Number: REF35
Hi Team,
my customer want a a 1.2V/1.25V Vout and ~1.5Vin, do we have recommendation? I see we newly released REF35 but datasheet mentioned it only support 1.7V Vinmin, so want to check with you if there is other recommendation or REF35…
Part Number: ADS8866 Other Parts Discussed in Thread: REF35 , , OPA333 , REF3330 Hi -
I am designing with the ADS8866 for a low power application. The TI REF35 looks like it would be the lowest power voltage reference to use.
I noticed in the ADS8866 the…
Part Number: ADS131A04 Other Parts Discussed in Thread: REF35-Q1 Tool/software:
#REF35 #ADC131A04
Hi Sir,
We are planning to use the ADS131A04 ADC converte r for PH & conductivity measurement for high accuracy & resolution
and for giving the 2…
Sorry,
I missed below information.
We are going to use REF35 series with 2.5V reference & the converter is 16-bit with target ENOB of 15-bit. Please advise ahead.
Regards,
jagdish
Part Number: OPA2188-Q1 Other Parts Discussed in Thread: REF35 , , OPA350 Tool/software: Hi team.
my customer is developing a precision 16bit data acquisition system with using a SAR adc without refence buffer, can you help me on how to select a proper…
Hello,
There are a few options to create a current source. LM4051AIM3X-ADJ/NOPB (LM4051-N) or LM4041CEM3X-ADJ/NOPB (LM4041-N) are good options to do so. An example using one of these devices can be seen in section 3.2 of this application note:
https:/…
Hi Wouter,
Not as a shunt device.
For higher performance you need to consider a series reference such as REF35 family.
REF35 Ultra Low-Power, High-Precision Voltage Reference datasheet (Rev. B) (ti.com)