Part Number: REF4132 Other Parts Discussed in Thread: LM4120 ,
Hi Team
Could you please tell me the wire number of REF4132B33DBVR and LM4120AIM5X-3.3/NOPB if you can share in this page?
Best regards,
Kenta
Part Number: REF4132-Q1 Other Parts Discussed in Thread: REF4132 Hi,
I have a question about the part number of REF4132-Q1. There are two suffixes about REF4132 in the package infomation, one is REF4132A and the other is
REF4132B, but I can't find…
Part Number: REF4132 Hi All,
I have a question about REF4132.
If VIN has already been input, I think that it is possible to input to EN with resistive voltage division. is my understanding correct?
Also, according to the data sheet below, the…
Part Number: REF4132 Hi All,
I have a question about the Load Transient of the REF4132.
The waveform is the result of -10 mA to + 10 mA, but if it is 0 to 10 mA, what is the waveform like? Does the output voltage fluctuate because there is no switch…
Part Number: REF4132-Q1 Hello. I am looking for a suitable second source for our design. In this circuit, the REF4132A40DBVRQ1 (reference 4.096V) is the EN pin to enable the output. Can this pin be left unconnected? Does it have an internal pull up/down…
Hi Wang,
Just for clarify here, are we referring to the REF4132B25DBVRQ1 or REF4132B25D ? As this is a BMS application I am assuming the automotive grade device will be used.
wang nanhan said: 1. is this OK to get high accuracy for trigger? <1% all…
Part Number: REF4132 Other Parts Discussed in Thread: ADC128S052 , LM4128 , LM4132 Hi All,
I have a question about LM4128A and REF4132.
(1)The recommended reference IC when using the ADC128S052 is LM4128A as a result of checking with ADC-TO-VREF-SELECT…