The reason I did not recommend the LM4140 is because it only works from 0C to 70C. The ADS1271 is usable in a longer temp range. If this ADC is only going to have a ambient temperature between 0C to 70C, you can use LM4140.
I prefer the REF50 due to…
Hi Andrew,
Use the EC table for 10 ppm/C for SOIC8. The REF50 used to be offered in MSSOP and that package had a 5ppm/C LTD after 1khr. The datasheet needs to be updated to reflect the current LTD.
Part Number: LM4140 Other Parts Discussed in Thread: REF50 Is there any data how LM4140 performs under 0 C? The exact temperature I'm interested in is -15C.
Thanks!
--Juha
Wen,
You're right, REF5045 is not mentioned for some reason. I'll look into this offline, but meanwhile, please consult the REF50-Q1 datasheet , where you can see that the typical will be 4.5 V as you mentioned.
Thanks, Abhinav.
Other Parts Discussed in Thread: REF50 We have a question about REF5025.
Please tell us the difference about these IC.
REF5025AID
REF5025ID
Best regards,
Takahiro Nishizawa
Part Number: ADS7950 Other Parts Discussed in Thread: REF50
Hi, I have some question about REF of ADS79xx series. I would like to confirm how to select an external reference voltage device. ①Does the REF pin need a device that can drive more than ±10mA…
Other Parts Discussed in Thread: REF50 Hi Team,
Customer need a voltage reference with high accuracy and good stability. Does TI have a voltage reference chip with an accuracy outperforming one out of 10,000?
Thanks.
Hi Vairavan,
I would suggest to use TINA-TI to solve the op amp equation or else look into Howland current source for something similar..
I cannot help you with manually solving it. I also cannot provide the values of R1 and R2 which are missing in…