Part Number: OPA350
Hello,
I'm reading Tips and tricks for designing with voltage reference ( SLYC147 ), where an OpAmp ( OPA350 ) is suggested as buffer for REF50xx after a RC filter. At the output of the OpAmp, a capacitor with a series resistor (that…
Part Number: REF5030 Hi,
Regarding the spec below, there's no additional explanation on test condition.
Is the maximum value just for at 25 degree C? or does it cover the full temp range(-40 to 125 degree C)?
Regards,
Go
Part Number: REF5030 Hi,
VIN <Vout may occur when the power is turned off. Is the device damaged? Is a protection circuit built in?
Customers may be too concerned about this question.
Best regards,
Hiroshi
Part Number: REF5030 Hi support team.
I have been inquired regarding changed spec of long term stability Spec in datasheet from my customer.
What the reason for difference of long term stability on VSSOP package between Rev_H and Rev_I?
Best regards, …
Part Number: UCC28070 Other Parts Discussed in Thread: REF5030 Ulrich,
we have been in contact for a PFC application with AC and DC input, where the controller is UCC28070 which is not designed for DC input. I have studied a solution that I would like…
Part Number: TMS320F28P650DK Other Parts Discussed in Thread: REF5030 , OPA350
Dear champs,
I am asking this for our customer.
It seems there are inconsistencies in the datasheet and in TI F28P65x control card/Launchpad schematic.
Questions:
1. What are…
Part Number: LAUNCHXL-F28P65X Other Parts Discussed in Thread: REF6230 , REF5030 , , TMDSCNCD28P65X Hi, Supporter.
In the user guide of " C2000 F28P65x Series LaunchPad Development Ki“, It says “ This REF6230 is not a recommended reference for…
Part Number: REF3430 Other Parts Discussed in Thread: REF5030 , REF54 , DRV8316 Hi team,
The REF3430 has a maximum capacitive load requirement of 10uf in the datasheet.
How is this parameter generated?
What happens if the load capacitance is greater than…
Part Number: REF5030 The REF5030 (or any of these REF50xx devices) state to use a 1-50uF output cap, connected from Vout to GND.
If i use a 10uF cap at the output pin, can this part support additional capacitance if it's not located directly at the output…