Part Number: REF5030A-Q1 Hello,
We've used REF5030A-Q1 as a 3.0V reference source for the MCU ADC, buffered by opamps. The output voltage however is incorrect, around 2.88V instead of 3.0V.
I've checked with the scope and there is no oscillation,…
Part Number: REF5030A-Q1 Hi,
My customer need assistance.
The output voltage of the chip REF5030AQDRQ1 is only about 2.8V, instead of the nominal 3.0V of the chip.Input voltage 3.3V, working environment temperature 20°C.The schematic diagram is shown…
Part Number: REF5030A-Q1 Hi, Voltage References team.
Do you have protection function about short to GND and short to battery(Vin) on the REF5xxx-Q1?
Thanks
Best Regards
Gerald
Hello Ozan,
I assume this is for the 16-bit option of ADC for F28386.
For 16-bit ADCs, REF31-Q1 is not the best option in terms of maximum load capacitance or performance. I would recommend one of the following parts:
REF5030AQDRQ1 (REF5030A-Q1…
Part Number: REF5050A-Q1 Other Parts Discussed in Thread: REF34-Q1 Tool/software: REF5050A-Q1 is rated for -40 to 125 deg. C, not sure if this device will function at -55 deg C ambient temperature or not?
Or do you have minimum -55 deg. C to 125 deg…