Other Parts Discussed in Thread: CC2650 I am pleased to announce that RemoTI v2.0.1 maintenance release is now available at http://www.ti.com/tool/remoti !
This version includes bugfixs (in the release notes) and support for the CC2650 Launchpad.
…
Hi Torbjorn,
This is exactly (almost) what we are trying to do also. I have two LP, once as RNP recipient, another as a RNP originator. Trying to get them to join together and send custom packet between.
The Recipient allowed the remote control to…
Other Parts Discussed in Thread: REMOTI , CC2650 , CC2620 I am happy to announce that RemoTI v2.0 is now available!
RemoTI™ 2.0 (Supports CC2620 and CC2650)
RemoTI™ 2.0 supports the backwards compatible ZRC 2.0 (ZigBee Remote Control) profile. …
Hello Torbjorn,
Thanks for the reply. It looks like the Target Emulator came with RemoTI 2.0.01.15, is v 1.06.05
Also, it might seems that it is expected to talk to a RNP recipient.
When trying to connect to a RNP originator, I get the following…
Dear Torbjorn,
Nice to hear from you again for this new post.
Thanks for your support. It worked.
Looking forward your continued support.
with Thanks & Regards
Jagdish
Program the following image to use the launchpad as recipient:
C:\ti\simplelink\rti_sdk_2_00_01_15\examples\hex\cc2650lp_rnp_rti_recipient_uart_super.hex
You can communicate with it using the CC2650RC, or any other ZRC2.0 compatible originator.
…
Part Number: CC2650 Other Parts Discussed in Thread: REMOTI , CC2620 Dear Friends,
My objective is to develop application in CC2650 with inbuilt stack and source code for customized application on a single chip. Is it possible.
I want to implement…
Other Parts Discussed in Thread: REMOTI Hello
I have doubt on the SupportedTargetTypes parameter from chapter 3.3.2 RemoTI API. 'Node Capabilities' corresponds to 'Node capabilities field ' in RF4CE Specification, DeviceTypeList to Device type list…
Other Parts Discussed in Thread: REMOTI , MSP430F5529 , CC2564MODNEM Hello,
I'm having a CC2564MODEM, RemoTI Target Board and MSP430F5529 LaunchPad
I’m wondeing if I:
Plug the CC2564MODEM module onto the Target Board
Attach Target Board(J4 Interface…