Hello Ofer,
the system you are planning would require LF tags that support the anti-collision process. TI is not offering LF tags that can fulfill this requirement.
HF transponders (13.56MHz), which are working according the ISO15692 standard, also offer…
Hello Josh,
The RF37S114 has the antenna included in the device packaging, and it is not meant to be used with larger antennas to increase the read range. This is a completed product to be used as is.
The die which was used to create the RF37S114 is: …
Part Number: TRF7970A Hi team,
Customer made their own NFC reader/writer using TRF7970A and Tags with RF-HDT-AJLS-G1, protocol is ISO15693. There're some Tags failed to be recognized correctly.
1. When use TRF7970AEVM read Tag1, the UID is E00…
Hello Bruno,
we have the RF-HDT-DVBB transponder that is a round transponder with a diameter of 22mm which is used in laundry applications.
This transponder is IP68 qualified. For more information please see the datasheet.
http://www.ti.com/lit/ds/symlink…
Madhuri -
this device (the RF37S114) has no external connection, its a complete tag.
Dimensions are: 4 mm × 4 mm × 0.66 mm ±0.1 mm
if you need die to connect to, same silicon would be www.ti.com/.../rf-hdt-ajle
Part Number: TRF7970A Other Parts Discussed in Thread: RF-HDT-DVBB Hi expert,
My customer tries to implement "time-out" processing in case no response, during writing command to Tag(RF-HDT-DVBB),
they can utilize Irq_noresp in IRQ Status Register…
Hello Taka,
you can find the description of the custom commands in the following Reference Guides:
http://www.ti.com/lit/ds/symlink/rf-hdt-ajls.pdf
http://www.ti.com/lit/ds/symlink/rf-hdt-ajlc.pdf
Best Regards,
Helfried
Part Number: RI-TRP-DR2B Please tell me whether RF-HDT-DVBB-B2 conforms to the following environmental standards?
· RoHS status (10 substances) · REACH status (191 substances) · Green status · IEC 62474
The status of the Web Page…
wow - great job - i would keep using the proprietary HW then -
using standard HW for this kind of application (i.e. Feig (LR2000 or similiar) and this same size antenna 300mm x 300mm, a tag this size would get between what is seen for 24mm circular and…