Part Number: CC110L Hello,
I am looking to work with a 400 - 410 MHz RF transceiver. I was wondering if the 433 MHz reference external components are perfectly compatible for the 400 - 410 MHz output range. If the answer is no, would someone help me…
Part Number: CC1310
I have two custom boards (design based of CC1310 LP) A and B. A chip antenna of 868 MHz is used in both boards. I have set RF parameters in smartrfsetting files like...
1) Frequency=868.000 MHz
2)Symbol rate= 50.000 Kbaud
3…
Part Number: TRF372017 Other Parts Discussed in Thread: TRF370417 , LMX2572 , TRF3705 , Hi, I am planning to use TRF372017 IQ modulator to generate 4.5 GHz signal from base band I & Q signal.
Does this IC support up to 4.8 GHz signal generation?
LO…
Hi,
With 48 kHz and 32 bits: 1536 kbps -> 192 kBaud.
Then the sensitivity would be at 868 MHz, 250 kBaud: -95 dBm
Using the TI Range Estimator: https://www.ti.com/tool/RF-RANGE-ESTIMATOR
Would expect a range in the region of 230-368m with the…
Part Number: MMWCAS-RF-EVM
Hi, I'm evaluating Radar SDK use case on MMWCAS-RF-EVM mounted on MMWCAS-DSP-EVM, specifically the use case radar_object_detect.
cascade_radar_object_detect.zip
These are my CC, coefficient.bin, coefficient script, and…
Part Number: AWR1642BOOST Other Parts Discussed in Thread: AWR1642 Dear TI,
I have two questions. The first one is related to the high accuracy demo visualizer. I was doing testing on short range with the AWR1642 (1 2 and 5 meters) I wanted to test…
Hi,
I addition to Ryans feedback, you can explore the range of various PHYs with the following tool: RF-RANGE-ESTIMATOR Calculation tool | TI.com
Is there a specific application you are targeting?
Regards,
Part Number: LAUNCHXL-CC1310 Other Parts Discussed in Thread: CC1310 Hi!
I have done measurements for RSSI / Distance with the CC1310. 120 measurements were made per distance, at distances between 2 m and 1.8 km, in Line-Of-Sight. But from ~220 m, the…
Part Number: IWR1443BOOST Other Parts Discussed in Thread: IWR1443 hello i have some problem about mmwave sensor
already i learned TI trainning of 'fundamentals of mmwave sensor'.
i wondering about range estimation. i want show the example about estimate…