The settings in SmartRF Studio are the characterized settings and will give you the sensitivity number that you can find in the data sheet.
You can use the range estimator to estimated the range you will get with the different modes:
RF-RANGE-ESTIMATOR…
Other Parts Discussed in Thread: CC1121 cc1121 tranceiver not able to receive the packet send, firstly i checked at transmitter end with 8051 interface to cc1121, here packet is transmitted and GPIO0 PIN asserts at start of transmit and Deassert at end…
Other Parts Discussed in Thread: LMH2120 , LMH2121 Hi,
Customer would like to detect and hold the peak signal that has spectrum from 1MHz to a few hundred MHz.
However, I believe LMH2121 could be operated from 100MHz to 3GHz. Are there any ways to…
Hi,
I have an outdoor application (can be used indoor as well) that should have max. 80m range. I designed a HW based on CC26xx module, but my modules' RF performance is not reliable after 15m.
I did test with CC2650EM + SmartRF. In general it seems…
Part Number: CC2538-CC2592EM-RD Other Parts Discussed in Thread: CC2538 , CC2592
Can I use cc2592 for both TX and RX communication in the same device. We designed 2 devices one (Device A) is based on cc2538 EM and the other one based on cc2538-cc2592…
Prafulla,
Thanks for you inquiry. I am not entirely sure what type of support you are asking, since chip antennas are quite straightforward to use as long as you follow the manufacturer's recommendations.
To have an idea about range tied to the antenna…
Other Parts Discussed in Thread: CC110L , CC3200 Hi everyone,
I intend to buy http://www.ti.com/tool/430boost-cc110l for my project. I have built a mobile robot, so I need to control wirelessly my robot in office environment which have a lot of obstacles…
Other Parts Discussed in Thread: CC3200 Hi,
The attached excel sheet helps to estimate a practical range estimation for indoor and outdoor radio links.
The outdoor is based upon Line-of-Sight (LOS). For the indoor estimation, construction materials…
Part Number: CC1352P7 Other Parts Discussed in Thread: CC1352P , CC1190 , , CC1310 , CC1312R7 , CC2592 , CC2590 , CC1101 Tool/software: Hi,
We have developed our board to a Wi-SUN application and we need to reach the maximum distance in a stable network…