Hi,
Refer to the Range estimator tool and there are some materials that can be included to act as attenuators: https://www.ti.com/tool/RF-RANGE-ESTIMATOR
However, with metal the main question will be if this is grounded or not?
Agree with the other…
Other Parts Discussed in Thread: CC2530 , CC2538 I read Excel sheet to estimate range for Indoor and Outdoor at http://e2e.ti.com/support/wireless_connectivity/f/538/t/375823.aspx. I find most of TI low power RFs are included in the excel but only CC2530…
This would be highly dependant on the indoor conditions, such as the type of walls and your choice of output power.
You can use our RF Range Estimator to calculate an estimate of how much one wall would attenuate the signal: https://www.ti.com/tool…
If I calibrate a LM20C sensor at T1=37°C and apply the offset to the 2 nd order transfer function, what can I say about the calculated temperature error at T2=25°C?
For the LM20C, the 2 nd order transfer function is
Vo = (–3.88 × 10–^6 × T^2) + (…
Other Parts Discussed in Thread: PCM5102 , CC1101 Hello Friends!
After many days reading through your helpful posts and wonderfulinformation within the TI.com site, I'm in need of some clarification and maybe a bit of help, if willing.
I'm a professional…
Other Parts Discussed in Thread: CC1200 , SIMPLICITI , CC1120 Hello !!
I need a radio that accomplishes this specs:
Long range -> indoor +- 500 m
915 MHz, must work in FHSS(35+ channels) or DHSS (for attending some regulations here in Brazil) -…
Hi Karthik, if you have the kits you can setup easy tests with the out of the box examples to get familiar with the network functionality. Please reach out once you have them and need help to set up a test. A good starting point is the SimpleLink Academy…
- I would recommend using https://www.ti.com/tool/RF-RANGE-ESTIMATOR to estimate the range you can get and see if this is what you need.
- Are you allowed to transmit with 1-2 W at your location with LRM?
With limited RF knowledge I would avoid FEMs…