Hi Kien,
The range will depend on the PHY you choose, but let's assume 1 km range (50 kbps PHY): 1000 m divided by 40 m is 25 devices per hop. 200 devices : 25 devices per hop = 8 hops.
(Or architecture only supports up to 6 hops but we're just trying…
For a range of 50-60 m, you should not need to use a P device. CC1311R3 would do the job:
CC1311R3 data sheet, product information and support | TI.com
Please also see the following:
RF-RANGE-ESTIMATOR Calculation tool | TI.com
Siri
Hi Danilo,
From the information I can find, the CC1120 has been successfully used in other satellite designs.
The customer can use this tool to estimate range: RF Range Estimator: https://www.ti.com/tool/RF-RANGE-ESTIMATOR
A Front End Module…
Hi,
The experiments you are performing with the antenna position and shape are quite normal when evaluating the best performing design for your product. The monopole antenna that you are placing on the edge of the board is a common topology that is…
Hello,
I am trying to change RF frequency range of my TSW1266EVM, by changing matching circuits at RF and LO.I am getting good dynamic range at default frequency around 2.1 GHz, but I need board center frequency around half this frequency 1.05 GHz.…
Hello JAN / Sabeeh,
I have two questions:
1. I see that CC3235 is not a concurrent dual-band device. Does it mean that transmission / reception on both 2.4Ghz and 5Ghz happens at the same?
So based on this assumption, can we use SOP0 and SOP1 GPIO…
Hi Rahul, Please have a look at our range estimator tool, and fill it with the relevant details of your application: https://www.ti.com/tool/RF-RANGE-ESTIMATOR
There is a Wi-SUN radio setting included as well. Regards,
Arthur
hey ,
I was working with configuring a source and a sink on a single device ie preparing a bluetooth intermediate device .
With some tweaks I am able to play audio in my headphones through the intermediate device .
no the problem is .. the sound…
Can you elaborate the range you expect? You can use TI RF Range Estimator to estimate radio range first. If you need more rang budget, you should consider using CC2652P, which contains PA and can output unto 20 dam tx power, instead of CC2652R.
Hi Manu,
Thanks for testing that. To add to this further, what settings did you use in SmartRF Studio and what estimated range do you get when using the RF Range Estimator that Arthur linked to?
For a general overview of PHY selection, please see…