For single hop distance, you can use RF-RANGE-ESTIMATOR to estimate it. When it's in real mesh environment, it will depends on how many hops you use. For feasible number of hops, my experiences is maximum 5.
Hi Rei,
In the article you've linked it says that the 200 m is for a single-hop (which is option ② ).
However, this is an optimistic estimate of the range (assumes line-of sight between receiver/transmitter). For a more realistic estimate of range…
Hi,
You can use either Fractus or Johanson Chip Antenna.
You can place either at the Corner or End Mounting configuration.
You can use our Range Estimator to estimate the anticipated range. I also recommend to test the Range on your Prototype…
Hi,
Q1: You can use LAUNCHXL-CC1352P-2 Reference design. Just exclude Sub-1GHz RF path. Everything else would be same. The following is the link.
2. You can use our Range Estimator for Range calculation. The following is the link.
www.ti.com…
The probable range can be estimated with: https://www.ti.com/tool/RF-RANGE-ESTIMATOR
Without knowing the settings it's not possible for me to know if 150 m is expected or not. Normally the output power is limited to lower than 14 dBm in the 433 MHz…
40 m is on the short side, even with 10 dBm.
Have you used https://www.ti.com/tool/RF-RANGE-ESTIMATOR to estimate the range with the settings you are using?
The settings you are using looks correct. Copy the 14 dBm setting from SmartRF Studio and…