You can use http://www.ti.com/tool/RF-RANGE-ESTIMATOR to estimate range with your settings and from this find which TX power you should have. Then you can test with these settings in the field to see if the estimate is correct in your case.
Hi,
Please look into the HW design guide:
https://www.ti.com/lit/swra640
Line of sight range will depend on what RF settings you use. We have a tool to calculate it here:
www.ti.com/.../RF-RANGE-ESTIMATOR
Hello Haggai,
Other than my earlier recommendations, I would recommend that you do more research about underwater communication methods, such as acoustic, light, and RF. Here are a few interesting articles that I found after a quick online search. IEEE…
- First thought is that 10 km is a bit optimistic, please use https://www.ti.com/tool/RF-RANGE-ESTIMATOR to estimate the range with your setup.
- It should not be required with an extra MCU. The CC1352R has SPI, UART etc which should enable you to communicate…
Hi
We do not have any devices that can do full duplex. For range, please see https://www.ti.com/tool/RF-RANGE-ESTIMATOR .
I will have someone from our HW/RF group comment on what data rates would be necessary to transmit voice
if you are only getting 1 m range with the 50 kbps settings, I suspect that there is either something wrong with your HW or there is a very strong jammer present at the same frequency as you are operating. Please use the range estimator to see what range…
The basics first:
4 km range point to point in an urban environment is not possible. Please take a look at https://www.ti.com/tool/RF-RANGE-ESTIMATOR . Note that to be able to transmit voice the datarate has to be in the range of 50 kbps or higher …
Hi,
If the Tx Power, sensitivity and Ant Gains are same in between 868 MHz band and 433MHz band then 433MHz covers more distance.
They can use 625bps, Legacy Long range mode. They can check SmartRF Studio under typical settings.
They can use…
Hi,
Start with typical settings in SmartRF studio and then export them to your project.
http://www.ti.com/tool/SMARTRFTM-STUDIO
The following link will provide a way to estimate RF link range.
http://www.ti.com/tool/RF-RANGE-ESTIMATOR
Thanks…