1.The example we provide supports one master,one slave,one passive. But theoretically, you can achieve multiple slave / passive devices by modifying the code, and the number depends on your system design.
2.The measurement result is highly related to…
1. The same PCB traced antennas cannot compete with external antenna.
2. OTA firmware update depends on your SW and it's not a problem.
By the way, you can use TI RF-RANGE-ESTIMATOR to estimate RF range.
Hi,
The range will not significantly increase by moving to CC26x2.
The range of BLE itself can be estimated with the RF-RANGE-ESTIMATOR tool. In the case of AoA, only the 1M and 2M PHYs can be used. When it comes to AoA accuracy, this will highly…
http://www.ti.com/tool/RF-RANGE-ESTIMATOR
The CC2420 is not included in this tool but find the setting that is closest to what you need.
Why CC2420? If you can choose I would start with a device that is a couple of generations newer.
- Sensitivity…
Hi Nick,
1- You could add an external antenna with a better gain than the existing PCB antenna.
2- GFSK modulation is mandatory for Bluetooth Low Energy. So as long as Bluetooth Low Energy is used, the modulation does not change.
3- The link budget…
Hi,
I recommend you first use our Range Estimator tool to estimate the Range. The following is the link to the Range Estimator.
You may need to use Range Extender ( CC1190) to boost Tx power and also for Rx Sensitivity improvement.
Please refer…
For some reason this case did not get mapped correctly internally, hence the delay.
- "Can you help support the edited PCB and Schematic": Please elaborate what you need help with.
- "Is there a reference circuit for a power amplifier": We have some…