Hi,
For a given situation the range for horizontal polarization is always less then vertical polarization and I'm wondering if is due to "destructive" interference from the two signal paths. I'm familiar with calculating site attenuation for open field…
Part Number: CC2652R Tool/software: WEBENCH® Design Tools Since cc2652R has horizontal antenna can u explain about the polarization of it . and which polarization will be best suited for horizontal antenna
Other Parts Discussed in Thread: AWR1843AOPEVM , AWR1843BOOST Tool/software: Hi,
i want to know can i trust mmwave sensing estimator results?
i searched for a measurement test data from for example AWR1843AOPEVM with clear mentioned complete config…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243 Tool/software: Hello,
In User's Guide, Radar spec related with detection range is not written. Please tell me detection range in each RCS and show me evaluation result if it possible…
Other Parts Discussed in Thread: CC1310 I'm using Sub-GHz modules for fully submersed (water) applications. I Was wondering if anyone has ever Estimated RF Range through a Water Medium, not a lot of info on the web and no tools exist since water is a…
Part Number: LP-EM-CC2745R10-Q1 Other Parts Discussed in Thread: LP-EM-CC2340R53 , Tool/software: Hi, TI:
When using the cc2745 for dual antenna CS ranging, the final estimated distances are not the same as the distances obtained from any of the four…
Part Number: CC1020
Tool/software:
I have 2 devices, both using CC1020 radio modules, operating in 900MHz band.
One functions as a TX (only sends RF msgs) and the other functions as a RX (only receives RF msgs).
Both devices are set to 911.222MHz…
Part Number: MMWCAS-RF-EVM Other Parts Discussed in Thread: AWR2243BOOST , AWR2243 Tool/software: Hello,
I want to test radar for an application, where an angular resolution in the range of the MMWCASRF-EVM is needed. The application only has to detect…
Part Number: IWRL6432 Good day,
According to the device errata, the IWRL6432 should be restricted from 58 GHz to 62.5 GHz.
Is there any indication when there will be a new version of silicon with this addressed and when one may be able to get samples…
Part Number: MMWCAS-RF-EVM Tool/software: i use many frames for the capture the drone data. then using post processing, i visualize the each frame using mmwave studio. in my situation , drone only flying towards the radar board ( it means drone velocity…