Hi,
If the Sensitivity and the Tx power are within the Specs then it should meet the expected Range.
Did you try our Range Estimator toll for estimated range? The following is the Link?
If the higher gain Antenna performs worse then it shows…
Please refer to www.ti.com/.../swra496 for details on the antennas we promote.
Also use www.ti.com/.../rf-range-estimator to estimate the range for your setup.
Hi,
1. Make sure the module you are using has a RF filter for 433MHz. You can use SmartRF studio with another sub-1G device to see if your frequency is at 433MHz. Use the Continuous RX tab with base frequency set to 433MHz and look at the RSSI. This…
The range estimator has been moved here:
The speed of sound is still very small compared to the speed of light so I doubt that you will see any issues. You can try to do the theoretical calculations.
1) Depends on the trace length. If the length is less than about 1/10 wavelength the line will not behave like a transmission line. I would select a trace width that is close to what a transmission line should be but if the line is short you can adjust…
Hei Kristoffer!
AoA relies on BLE 1M (or 2M) PHYs - Coded PHYs cannot be used with AoA. You may then want to verify using our RF-RANGE-ESTIMATOR what is the range achievable in your specific case.
To increase the range, you could increase the TxPower…
I could sound like the outdoor noise floor is very high.
As you can see when using this tool: http://www.ti.com/tool/rf-range-estimator , the range goes down if the noise floor is high. You can measure the noise floor using SmartRF Studio and using…
- You can estimate the expected range by using
- Before you calculate range you should measure the background noise where you do your test. In SmartRF Studio, set the launchpad to cont. RX and observe the RSSI. This test have to be done without a known…