Hi Wu Qiang,
intfMitigCfg is used during Range Processing to perform interference mitigation. To understand about interference estimation and mitigation, you can go through sections 28.7.3 Interference Localization, 28.7.4 Interference Statistics and…
Hi, Liang:
The demo will apply CFAR detection in range-Doppler heatmap. In this stage, we should only have unique peak for each range-Doppler pair. However, during angle estimation, another CFAR will run on angle spectrum, and that is when we can have…
Hi Felix,
Felix Doe said: The left hand side of each row is the matlab post processing using the calibration matrix that has been generated with configuration data of my own, short range configuration, the right hand side is the same data, but post…
Venkatadri Ji ,
The Inductance Measurements was done using standard LCR Meter Fully Assembled Motor (with Magnets): The inductance value fluctuates significantly, ranging between 21 mH and 60 mH. Stator Winding Only: The inductance remains stable at…
Part Number: HDC2010 Other Parts Discussed in Thread: HDC3020 , HDC3022 Hi sir
we need a sensor for extreme environments-
1.
Please confirm whether this sensor (HDC2010YPAR) can operate correctly within the range of 500 feet below sea level to 20…
Part Number: CC2652R Other Parts Discussed in Thread: CC2592 Hi Team, Continuing the discussion, As suggested we have tested the results. Kinldy find the attached test results in the document Home_automation_Range_test_report.pdf
Kinldy check and share…
Hi Nikileshwar,
Please see my response to your question below
1) how to choose eroe band and settling time for the loop coffeficients calculations?
Settling time is usually associated with 2% error band which has a relation to bandwidth as discussed…
Hi, there:
Sorry for the delay, please see my answers below.
1) How does data flow from the ANA subsystem to FESS (directly)?
The data from analog to digital is part of the ADC and digital front-end logic.
2) Is raw data from FESS stored directly…
Hi Danilo,
Question 1: Your RD-first strategy has a known limitation: near-stationary or very slow-moving targets.
TI's people counting demo actually uses the opposite order: Range → Static Clutter Removal → Angle of Arrival (Capon) → CFAR → Doppler…