Hi samhitha,
thanks
A. Mani D said:
b.max_range_detectable_object_fast_chirp_BF= 124.44m(for MRR mode mrr_config_chirp_design_MRR120.h)
c. max_range_detectable_object_slow_chirp_BF= 130.24m(for MRR mode with mrr_config_chirp_design_MRR120…
Part Number: ADS54J60 Other Parts Discussed in Thread: LMH5401 Our design has ADS54J60 with fs=1Gsps. The goal is to capture signals from 1st and 2nd Nyquist. Datasheet specifies that at 720 MHz, we should get ENOB of approximately 10.5 bits (table in…
Part Number: TPS22860 Hi, We are using TPS22860DBVR in one of our design where we require to monitor the battery voltage.
As per the datasheet, there are couple of graphs provided as shown below - which grpah we shall consider to estimate the leakage…
Hi Patrick,
I don't have an estimate of the output resistance, but with the 24VDC input, the system was drawing about 2A steady state. I would estimate the total output capacitance to be in the range of 800uF to 1000uF.
Hi Bowei,
Yes, you can output range profile data over UART - it does not require the DCA1000EVM. TI provided demo firmware outputs multiple TLVs at once over UART, so you can save the data using the mmWave Data Recorder or Industrial Visualizer (found…
Part Number: AWRL1432 Other Parts Discussed in Thread: , IWRL1432 Hello TI Team,
I am evaluating the AWRL1432 radar sensor for automotive short-range radar applications and would like to understand its practical RF performance and supported use cases…
Part Number: IWRL6844 HIi experts,
Now my customer inquiring which comparison criteria is important to select mmwave IC. As I know, our mmwave IC is superior human detection algorithm to others.
Regarding hardware, which RF factors have big implact…
Hello,
Sensor Installation: I have set the sensor height to 1.3m with a 0-degree tilt angle. (The default recommendation is 2–2.5m at a 2–3 degree tilt). Do you foresee any issues with this specific installation height and angle?
No issues
Range…
Hi Cesar, Thanks for your reply. After further review, I located the MmwDemo_addDopplerCompensation function in the dss_data_path.c file. Based on the code structure and documentation, I understand that this function handles Doppler phase compensation…
Part Number: BQ24600 Other Parts Discussed in Thread: BQ24610 I am using BQ24600 to charge Li-ion batteries in a dual-channel charger design. I would like to understand how the IC behaves when the input voltage is reduced and whether it automatically…