Hello Chris,
RI-STU-MRD2 is delivered by TI as a component to be assembled into end-use systems. As a result, CE compliance is not applicable. TI provides the material content compliance data required to document the RoHS requirement of CE compliance…
Other Parts Discussed in Thread: RI-SMD-MRD2 We are using the RI-SMD-MRD2 and is there any issues we need to consider when applying potting compound material around this assembly? The potting material will coat the assembly. We need to do this due to…
Other Parts Discussed in Thread: RI-SMD-MRD2 In the "RI-SMD-MRD2: Detect absence of antenna" forum answer it indicates that the "For the SIG_IN_0/1 pins the Vin_High_Min = 2V and for Vin_Low_Max = 0.8V. It is a direct input to a 3.3V supplied 74LVC244…
Part Number: RI-STU-MRD2 Other Parts Discussed in Thread: MRD2EVM Hi
Can you please confirm SKU RI-STU-MRD2 is CE and if YES, please provide the CE/EU Declaration of Conformity?
I could not find the info on the Texas instrument website.
Thank you very…
Part Number: RI-STU-MRD2 Hi i have a few questions regarding frequency change on Microreader RI-STU-MRD2
In the document scbu049: 6.4.3.26 Execute C-Trimming (Command 0x43)
This command starts a C-trimming sequence to adjust the transponder resonance…
Part Number: RI-SMD-MRD2 Other Parts Discussed in Thread: MRD2EVM Hi There,
We are wondering if it is possible for the RI-SMD-MRD2 to detect the absence of an antenna by monitoring output power or voltage levels? We are trying to figure out a way to…
Part Number: RI-SMD-MRD2 Other Parts Discussed in Thread: RI-STU-MRD2 , MRD2EVM , Hi team, Our customer is using the RI-STU-MRD2 reader module, however, upon connecting the board, the software does not recognize it. An error message "No reader identified: Connect…
Part Number: RI-SMD-MRD2 Tool/software: Code Composer Studio Dear Sir,
I need to interface the RI-SMD-MRD2 from a DSP through a serial interface.
The DSP has to run an algorithm developed on a WIN-PC with mathlab.
It would be great to have the source code…
Other Parts Discussed in Thread: RI-STU-MRD2 Hi team,
Could you make sure the weight of RI-STU-MRD2 ?
We found the weight difference as below.
Commercial invoice : 1g
Reference Guide (Table 3, page 12) : 5g
Reference Guide : https://www.ti.com/lit…