Part Number: RM44L520 Other Parts Discussed in Thread: HALCOGEN Hello all,
I have been having a bit of trouble getting the Pin ID from the ADC pointer. Right now I am using ADC1 Group 1 and have Pin 6 and Pin 3 enabled. I then use the following function…
Part Number: RM44L520 Dear all,
I design a PCB to be compatible with both MCU RM44L520APZ and TMS570L0332.
To get some source code parts compatible with both MCUs, I need the confirmation that the following instruction will not lead to unexpected behavior…
Part Number: RM44L520 Hello,
I am attempting to port over the RM48LX SD Card project into my project. I have been following the guide I liked below:
https://community.element14.com/members-area/personalblogs/b/blog/posts/ti-hercules-launchpad-using-an…
I recommend performing PBSIT test for all the memories used in your application during boot-time. Running PBIST on memories is destructive and you should backup your data and runtime information when performing a PBIST periodically.
If your application…
Part Number: RM44L520 Other Parts Discussed in Thread: HALCOGEN , Hello,
I am trying to configure SCI3 to communication with another internal device using pins 36,38,35, and 34. I have configured them all in halcogen under the SPI3 tab and have selected…
Part Number: RM44L520 Other Parts Discussed in Thread: HALCOGEN Hello, I have posted the first portion of this to the FreeRTOS Fourms and it seems that this issue is likely due to some issue in my interrupt configuration. Please see below:
I have a program…
Hi Andrew,
Yes, you need to enable the channel 10 (HET High):
and channel 24 (HET LOW)
The interrupt Eof Duty 0 is configured as "High Level", but the Eof Period 0 is configured as "Low Level"
Part Number: RM44L520 Other Parts Discussed in Thread: HALCOGEN Hello,
I've been having a bit of trouble properly configuring a pullup resistor in halcogen. I have set the direction of the pins that are in use to input in halcogen, selected the pull up…
Part Number: RM44L520 Dear Champs,
My customer is using RM44L520 for their functional safety MCU in Robot system and also using TPS65381 for PMIC.
Due to delivery issue of TPS65381, they are looking for other PMIC can be used with RM44L520 for functional…
Part Number: RM44L520 I've been having some issues with a project I am working on and figured somebody here might be able to provide some insight. The project I am working on is using the TI RM44L520 and I am currently trying to configure a 4-20ma chip…