Part Number: SA555 Other Parts Discussed in Thread: LMC555 , TLC555 Hello TI Team,
I designed the SA555 as a power ON delay cicuit.
SA555 is supplied with 12V. The SA555 is 16-17°C hotter as the environment.
After the delay time the IC is…
Part Number: SA555 Other Parts Discussed in Thread: TLC555 Hello guys,
One of my customers is considering using SA555 for their new products.
They want to achieve very long timer using SA555 with Figure 9 Circuit for Monostable Operation on page 10…
Part Number: SA555 Dear Sir,
Can you provide the relevant documents to confirm item SA555DE4 is same as SA555D?
Please reply to my e-mail: maggie@komori.com.hk
Best regards,
Maggie
***********************************
KOMORI ELECTRONICS (HK…
Part Number: SA555 Hello all,
I want to use the SA555 in Monostable Operation with 5V supply. A typical circuit is shown in datasheet in figure 9. In this circuit, the Discharge Pin is directly connected to the capacitor of the RC network. In this schematic…
Part Number: SA555 Hello Sir,
my customer needs to know the reflow temperature profile for the SA555DR.
Could you please provide specs, guidance or any other helpfull information.
Thanks in advance!
BR,
Alen
Part Number: TLC555 Other Parts Discussed in Thread: SA555 , LM555 , LMC555 Hi,
My customer uses TLC555IDR, instead of SA555DR.
*1. According to datasheet of SA555, A bypass capacitor is highly recommended from VCC to ground pin; ceramic 0.1 µF capacitor…
Part Number: SA555 Other Parts Discussed in Thread: TINA-TI
Dear TI,
I'm using the SA555 timer to generate a PWM frequency with the circuit shown below. The clock input is generated using another SA555 IC with Ra=Rb=12k and C=20nF.
To vary the…
Part Number: SA555 Dear TI Team Guys:
Custom use SA555 as pwm generator to control DC Motor. the schematic as fellow.
When testing the pcb , Speed form 0 position to 1 position, SA555 fault the output voltage always be low .
Change a new SA555 …