Hello Team,
This is a unusual request. I have a customer who is considering using the SD3GDAEVK for their product evaluation. They have requested the top and bottom views pictures so that they can get an idea of how the board looks. They have access to…
Other Parts Discussed in Thread: LMH0344 Hi,
I got the below question:
We bought the SD3GDAEVK SDI reclocker EVB, when we tried to evaluate it we encounter the following issues :
In general the EVB does not work
After some debugging we found the following…
Part Number: LMH0344 Hi all I'm using lmh0344 as 3g-sdi input equalizer.I have some questions as fllows The inductor of the network is 6.2nH on SD344EVK,with a 0.5pF capacitor in parallel with it.while the inductor is 6.8nH,without capacitor on SD3GDAEVK…
Hi Jordan,
The SD344EVK board is no longer in production. For our latest recommendation, we recommend a value of 6.8 nH that corresponds with the value used for characterization to achieve improved Return Loss performance. Please refer to the following…
Just spotted another point. In the datasheet, the input filter has a 3.9uH inductor across the 75R resistor. The SD3GDAEVK evaluation kit design uses a 6.8uH inductor. Is there some significance to this? Which is the "right" value to use please? Thanks…
Hi Takushi-san,
The testing that KDS ran using our SD3GDAEVK was conducted using a 18pF loading cap. That is the load capacitance we would recommend.
Thanks,
Kevin