Hi Kevin, Thank you for considering it. I noticed that I cannot use the old firmware on the newer GUI. At this moment, I do not have any problems but in the future, my customer may experience an issue and I wouldn't be able to replicate the problem. …
Hi Jimmy,
Jimmy Lai said: May I ask about the in what situation would the I2C1_Master start communicating to Slave IC? And how to let the I2C _Master work? Thanks a lot.
This app note here should help!
I2C with the TPS65988: https://www.ti.com/lit/an/slvae18…
Hi Saito,
Assuming the cable type is "Passive", then as shown below the VDO version will be set to 1.0.
In the GUI Config Tool there are some settings you can change to set the VDM version to 2.0. First check in PD3 Configuration Register…
Hi,
If you are referring to Equation 4 then the ESR is that of the polarized output capacitor.
I'd guess that the switching frequency would be 400kHz but let me reassign to the PSIL-PI group to have the appropriate apps engineer comment on what the internal…
Art, this particular design does appear to have been removed from the website and is now obsolete, with no replacement being offered at this time. The design was originally released in May of 2019 by the PSIL-PI team in APP.
Best Regards
John Fullilove…
hi team
I have a question in the paper of " Fast role swap power architecture white paper " which was wrote by Jacob Ontiveros from PSIL/PI/Applications.
Firstly, thanks very much for Jacob's paper.
In the equation 1, on page 6, why the R…
Part Number: TPD6S300A Hi, PSIL/PI support team
Customer ask me about the handling on N.C pin(16)/(17).
The datasheet mentions as follows
What will happen if N.C pin is floating?
Where is NC pin connected inside? Is it a substrate or other place?
…
Hi Jon,
Kedar is no longer within the PSIL-PI team and has moved over to our battery charger group. I'll be taking over in supporting this issue. Would you be able to send over both project configuration files for the TPS65981 and TPS65982 from the above…
Hello Bogey. This is a very important development for Power over Ethernet (PoE)!
You can read more about it under FAQs - published here:
e2e.ti.com/.../design_notes
To re-post the main comments:
What’s the difference among IEEE 802.3af, IEEE 802.3at…
Thanks kb
As I said before, I have approached two methods for running vision_apps based on QNX+RTOS mode.
First, I build the SDK QNX 7.0 with JBN29 QNX BSP version (Not modify : BUILD_CPU_MCU1_0 build flag from “no” in the vision_apps/vision_apps_build_flags…