Part Number: SENSOR-CONTROLLER-STUDIO Dear All,
We are looking for alternate Part for this TPS26631PWPR. We need experts suggestions in order to keep our production ON...
Part Number: CC2642R Hi,
I tried to create an example just with the COMPA and the COMPA event trigger. To do that a linked the COMPA to the DIO30. DIO30 is an ADC powered with 3.3V. My trigger is set to occurs when the DIO30 falling edge.
This is my code…
Part Number: CC2642R Hi,
I created a project in SCS to use the COMPA and COMPA event trigger. To do that a linked the COMPA to the DIO30. DIO30 is an ADC powered with 3.3V. My trigger is set to occurs when the DIO30 falling edge. Everything works fine in SCS…
Part Number: SENSOR-CONTROLLER-STUDIO Other Parts Discussed in Thread: CC1352R Hi,
I have a sensor controller application running execution code and event trigger code, and I want to check if the processing takes too long to reset everything. I'm trying…
Part Number: CC2642R Other Parts Discussed in Thread: SIMPLELINK-CC13XX-CC26XX-SDK Hi,
I'm new using the sensor controller and sensor controller studio.
I need a fast response when the ADC exceeds the high threshold. I think the example ADC Windows…
Hey Barrett,
I have the hardware but am not familiar with Sensor Controller Studio, can you send me a minimal set of projects to reproduce this behavior?
Part Number: CC1310 Hi ,
We have an old released product based on CC1310 and it’s sensor controller was compiled with sensor controller studio version 1.5.0.188.
During fixing a bug in the sensor controller code we could not find the original sensor…
Hi Murugan,
Which version of Simplelink CC13X0 SDK are you using together with Sensor Controller Studio? Also have you tried importing the example generated by Sensor Controller Studio into CCS? A few configurations have to be done by the MCU before the…
Part Number: LAUNCHXL-CC1312R1 Hi
I am using the ADC to sample the Sine and Cosine is there a fixed point CORDIC available for Sensor Controller Studio or failing that a fixed point ATAN2 any help would be appreciated.
Regards
David