Part Number: SG3524 Other Parts Discussed in Thread: DRV8251 , hi ,
I want to design a compressor that conforms to two different architectures
item1 have 3pin input,The middle tap of the coil is connected to 12v
item2 have 2pin input,
I want to…
Part Number: SG3524 Tool/software: We are planing to design isolated dc-dc converter using push pull topology and specification are input voltage 5V output 3.6 power 60w, can you provide any reference design .
Part Number: SG3524 Tool/software: We are designing the DC-DC converter through using the pulse width modulation (SG3524N) with out the load we are getting the output, but when connected the load its dropping the voltage, below circuit we are implemented…
Part Number: SG3524 Hi,
We have been sent a SG3524 based , opto isolated pushpull to work on.
Its 24vin and 24vout and 160W
The opto is connected to the COMP pin in common emitter connection. The error amp + input is connected to a 2v5 divider…
Part Number: SG3524 Hello team, My customer has a question about SG3524 dead time. They designed the following schematics. /resized-image/__size/808x549/__key/communityserver-discussions-components-files/196/7635.sch.png
The dead time of the output…
Hi Steve,
Per the attached circuit:
The value of RT is 10k and the value of CT is ~1000pF. A small amount of parasitic capacitance is added to CT because these parts are in a socketed breadboard for evaluation.
To keep the voltage on OSC OUT from…
Part Number: SG3524 What should be the spec of SYNC signal, so SG3524 can work with EXTERNAL SYNC? Is there any REF-CIRCUIT for SYNC? What should be the MAX on time and off time of SYNC signal?
Part Number: SG3524 Good morning,
I am an engineering and was looking for a missing information in the datasheet of the chip SG 3524. I need to know the current/power comsumption of the chip as well as the current peak that each of the BJT transistors…