Part Number: SG3524 WE PRODUCE DC DC CONVERTER CIRCUIT USING UC3524AN PWM REGULATOR.WE NEED THE SOIC 16 PACKAGE OF THIS PRODUCT WITH NEW REGULATION.BUT ON THE MARKET THIS PRODUCT IS PROVIDED SG 3524.WHAT WILL I HAVE PROBLEMS IN ALL INVERTER CIRCUITS WE…
Part Number: SG3524 Dear TI Team,
I am looking for a product of the specifications below.
I could not find it on the TI site and would like help.
Spec :
1. bandwidth : 4Mhz up to 10Mhz
2. Pulse width : 200ps under
only need to spec the…
Part Number: SG3524 Hello
I am using the SG3524 with the pin 1 connected to 9 and adjusting the PWM with the voltage on 2 ( potentiometer ); I join the drawing ( Dont' pay attention on PNP and NPN for Mosfet, it is N and P chanels..mistake )
Now,…
Part Number: SG3524 Other Parts Discussed in Thread: UCC2808A-1 , UCC28C40 Using the SG3524 to drive Mosfets in a push pull configuration to power a center tapped transformer. Works great at 5 khz but when trying to operate with our new 200 khz transformer…
Part Number: SG3524 We are qualifying PWM controller from TI MPN:SG3524N for obsolete part SG3524BN from Microsemi.
Datasheet and technical parameters are matching with older part. However, functionality wise TI SG3524N IC is not working for older…
Part Number: SG3524 Hi Ashish,
We are qualifying PWM controller from TI MPN:SG3524N for obsolete part SG3524BN from Microsemi.
Datasheet and technical parameters are matching with older part. However, functionality wise TI SG3524N IC is not working…
Hi there Ronald,
My internet connection has been down for the past five days. In the meantime I purchased a couple on new SG3524 chips. These are working and at the low frequency that I wish to work at I am able to modulate the relays as I wish. I am…
Other Parts Discussed in Thread: SG3524 I am using SG3524 to control a half bridge inverter or a buck converter.
On Pin7 CT (saw-tooth signal), on the falling edge, I see a jitter of 1.5 uS max, even if there is no input signal at Pin2.
This is constant…