Part Number: CC3235MODS Hello Experts,
I receive some inquires from customer. (Those inquiry are related to the following E2E thread : https://e2e.ti.com/support/wireless-connectivity/wifi/f/968/p/949732/3511063#3511063 )
Customer is able to request TI…
Hi Surendra,
Surendra Reddy said: Please let me know "How to flash MCU image with certificate catalog provided at <SIMPLELINK_CC32XX_SDK_INSTALL_DIR>/tools/cc32xx_tools/certificate-catalog/
You can refer to the Vendor Device Authentication with…
Hi,
For the OTA image signature the simplelink only supports a single certificate and not a chain.
The signature must use EC with the exact curve as defined in "<SDK-ROOT>/docs/simplelink_mcu_sdk/Over_The_Air_Update_Guide.html" or in chapter 4…
Part Number: CC3235MODS Hello Experts,
We receives some inquiries about Japanese RF certification from customer.
1. Customer knows CC3235MODS is certified for FCC, IC/ISED, ETSI/CE, MIC(TELEC), and SRRC. According to Certification reports ( https://www…
Hi Sundar,
We are not supporting the short lived access but they used to have the option to select the "No Expiration". If they don't have it now we will recommend that you will use a different server.
Old DropBox App should still work…
Hi Miriam,
1) Which version of the SimpleLink CC13xx/CC26xx SDK are you using?
2) In the host test example, the UART is used to receive HCI commands. If you want to use a UART for display, I would recommend you set up the second UART on the LP for this…
Hi Robin,
I believe this points to an issue with your setup. You can download and review the Launchpad test reports here: http://www.ti.com/tool/SIMPLELINK-CC3XXX-CERTIFICATION
Thanks,
Alexis
Part Number: CC3135MOD
Hi, I just want to clarify some things. Document: SWRU455M – FEBRUARY 2017 – REVISED OCTOBER 2020
From the userguide, it read: • Client Authentication If the server requires client authentication, the following files are…
Hi Karthik,
Can you try using the default dummy certificates provided with the demo? This will help isolate the problem.
If the demo works by default, then you should ensure that your certificate chain is valid according to the SimpleLink Wi-Fi Certificates…