Hi Yan,
Thanks for the update!
Personally, I have only used the DCC bin files, but I am not aware of any issue with the first way. You may use the DCC bin file for simplicity.
It is possible that "mesh.txt.bin" is not in the right format as MeshToBin.pl…
To convert unidirectional signals from 3.3 V to 5 V, you could also use a buffer with TTL-compatible inputs, e.g., SN74AHCT244. (This optimizes for price, not for BOM simplicity.)
If you have unidirectional signals in different directions, the best choice…
Part Number: PHYTC-3P-KIT-AM64 Hello experts,
I'm trying to execute a data transfer from A53 core to R5F core (using IPC) and then from R5F to a peripheral using SPI. To do so, I've combined two examples IPC_rpmsg and mcspi_performance_32_bit. But…
Part Number: UCC23514 Hi,
I am designing a boost converter with SIC schottky diode and SI mosfet for simplicity. I want to know how to rationally choose which transition of mosfet should be higher or lower. the reverse recovery of SIC diode is very less…
Hey Madhusudhan,
As mentioned in the Bosch MCAN User Guide , when the Rx buffer is used to receive data, the Standard Filter Type (SFT) register is ignored and only a single ID can be received by a single buffer. You would have to setup multiple buffers…
Hi Pieter,
Pieter Winter said: Yes. I rounded down for simplicity when I originally mentioned 190 MHz.
- Just wanted to be sure.
Pieter Winter said: To be clear: Are you talking about CPout pin, 25?
- That is correct.
Please monitor VTUNE over temperature…
For simplicity and finding the root cause to the issue can you remove/comment out all code pertaining to HRPWM and syncronizations just configure action qualifiers and see if the epwm outputs work as expected ?
Can you send me all the epwm only configurations…
Hi Joshua,
One of my original reasons to set my choice on MCF8315A was the supposed simplicity in the BLDC setup. Unfortunately, I do not have a recording oscilloscope to take those readings.
Looking at what happens, during MPET I can see a smooth widening…
Hi Nozomi,
It looks like you asked the same question in this thread, for simplicity we will close the duplicate thread and any additional follow up can be done in the below thread instead.
https://e2e.ti.com/support/interface-group/interface/f/interface…
Good day Walter, I thank you for your kind response. Well, the circuit I provided using the LM40401 seems to work OK in all aspects except the MOSFET gate does not go to ground and is lifted to about 1.5V due to the LM4041, I thought this may be the operating…