Part Number: CC2652R Hello,
I'm working with a SoC CC2652R and I'm using CCS Version: 10.3.0.00007 and simplelink_cc13x2_26x2_sdk_5_10_00_48.
I need to import an ONNX file containing an artificial neural network and process it in the microcontroller…
Part Number: BQ76PL455A-Q1 Other Parts Discussed in Thread: TEST , BQ40Z80EVM-020 , BQ76PL455A Hi,
I manage a modeling and data science team for a company that develops next-gen Li-ion batteries for EV applications. We are looking to build a BMS in order…
Part Number: AM5728 Hello,
I downloaded the latest PLSDK 6.03.00.106 image and created an SD card to run the TIDL ssd_multibox example. However, trying to launch any of the matrix gui examples for me just crashes. Launching the ssd_multibox example returns…
Hi,
I am Ananth From Vortex Engineering Pvt Ltd Chennai. We are planning to select the processor with following Spec
Architecture :64 bit
Flash memory : Greater than 1MB
Operating Frequency : Minimum 500 MHz
Should support with ML and other applications too…
Part Number: TMS320C6748 Hi,
I am using the TMS320C6748 LDCK with XDS110 Debug probe. I am perform A sampling of DFT of 1000points with timing shifting. I am looking at the tensorflow lite library but i am not sure how to port the library to the board…
Part Number: TI-RTOS-MCU
Is there any tutorial/guide/information on how to deploy a ML model in a CC3220 ?
the process goes like this:
CC3220 receives 10 readings from different type of sensors
the readings are passed to the ML inference function
blink…
Part Number: AM3354 Can the GPU in the AM3354 be used for ML or AI applications?
We found this link ( https://www.ti.com/processors/digital-signal-processors/libraries/open-cv.html no GPU acceleration unless we use AM572x or 66A2x?
Thanks, Nick
Part Number: SITARA-MACHINE-LEARNING
I want to interface a camera having CameraLink interface with Sitara AM5728 processor. Kindly help me how should I do that?
1) Do I need to use some special interface IC? If yes, kindly tell me its part number. Also…
Part Number: TMP117 Other Parts Discussed in Thread: TEST hi Team
does TMP117 require calibration? observed that the temp report is off and takes time for it to become stable.
Thanks