Part Number: SK-AM62-LP Other Parts Discussed in Thread: UNIFLASH Tool/software: Hi Team,
I am using uart_uniflash.py file for flashing the u-boot images to OSPI Nand flash and these are my configuration file as show below.
and I'm downloaded, using…
Part Number: SK-AM62 Tool/software: I am using the SK-AM62 E3 board and attempting to boot from eMMC after flashing U-Boot and the OS image. Here’s the process I followed:
Initially booted the board using an SD card.
Ran the following commands…
Part Number: SK-AM62 Tool/software: Hi,
I have written a custom UART driver using 8250 core structure. if I try to write from device I can see following logs coming up on terminal
omap_i2c 20000000.i2c: controller timed out
tps6598x 0-003f: tps6598x_interrupt…
Part Number: AM625 Other Parts Discussed in Thread: SK-AM62 Tool/software: Hello!
On SK-AM62, can you replace DDR4 directly with LPDDR4 without changing the hardware circuit? If it can be replaced, can you recommend a feasible LPDDR4?
Part Number: SK-AM62-LP Tool/software: Hi Team,
I want to change the emmc partition like below
=> mmc part Partition Map for MMC device 0 -- Partition Type: DOS Part Start Sector Num Sectors UUID Type 1 2048 32768 b23a7979-01 06 Boot 2 34816 524288…
Hello, Refer to this thread for a simple example of enabling a GPIO on the User Expansion Header: https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1268671/sk-am62-using-the-gpios-in-the-40-pin-user-expansion-port/4804378
You can…
Part Number: SK-AM62-LP Other Parts Discussed in Thread: AM62P5 , , UNIFLASH Tool/software: SOC: AM62P5
Board: SK-AM62-LP
Ref URL: https://software-dl.ti.com/processor-sdk-linux/esd/AM62PX/10_00_07_04/exports/docs/linux/How_to_Guides/Target/How_to_boot_quickly…
Part Number: SK-AM62 Tool/software: Hi,
I want to understand more about _UART_TIMEOUT Registers mentioned in AM62x TRM. I am not able to see any references to it in kernel sources.
I can see some reference to character timeout indication detection in UART_IIR…
Hi Jyo,
Jyo Sar said: Flashed the SD card with tisdk-default-image-am62xx-evm.rootfs.wic.xz image.
Please provide the details where you get this wic image.
Jyo Sar said: After flashing the image to SD card , changed the below file name Rename tiboot3.bin…