Yong Hui Liew said: When I tried to "test connection" it mentioned that the IR and DR scan failed and is unable to circulate bits.
This is a low-level JTAG communication failure. See the section called "Invalid data read back" in the article…
Part Number: SK-AM62 I am attempting to add a CAN transceiver to the boar using J9 pins 16 and 22.
Once done How do I enable the MCU_MCAN0 interface to make use of it
Part Number: SK-AM62 Hello,
Where can I confirm that the mode 0 and CS0 are used by default in the SPI back up boot configuration? They are configurable for Primary boot, but there is no reference to what they would be for the backup (Section 5.4.1.4…
Hello Vic,
Ok. Setting some expectations here:
1) If you are not testing with the same hardware setup that TI uses to test, I am not going to be able to try to replicate your results. (i.e., if you are not testing with SK-LCD1 ). This will limit the support…
Part Number: SK-AM62 I am running the following for TI-SDK 9.00.00.03:
cd tisdk/build . conf/setenv export TOOLCHAIN_PATH_ARMV7=$HOME/gcc-arm-9.2-2019.12-x86_64-arm-none-linux-gnueabihf export TOOLCHAIN_PATH_ARMV8=$HOME/gcc-arm-9.2-2019.12-x86_64-aarch64…
Part Number: SK-AM62 I am following steps mentioned in this link - Overview_Building_the_SDK for building the SDK. I am facing build errors and herewith attached the log of the build. Please let know how to resolve this build error.
8484.log.txt
Part Number: SK-AM62
Hi Everyone,
I have used for SK-AM62 E3 revision sitara board, I have edit k3-am625-sk-inmate-demo.cell file how to edit tell me
Regards,
Veerapandiyan V.
Part Number: SK-AM62-LP Hi
I want to configure several GPIOs as interrupt pins.
On dev.ti.com, I can only find options for setting Pull UP/Pull Down resistors for GPIOs.
Do I need any other configurations?
Hi Veerapandiyan,
For MAIN_I2C0, can you currently check the jumper wire connections from SK-AM62 to MPU 9250 and write it down for me, I know I have already given the connections but please check the connections you have right now and list them down…