Part Number: SK-AM69 Other Parts Discussed in Thread: AM69
Hi, I'm using ti-processor-sdk-linux-edgeai-j784s4-evm-10_01_00_05-Linux-x86-Install.bin on SK-AM69.
When I run the folowing pipeline: gst-launch-1.0 rtspsrc location=rtsp://192.168.109.242…
Part Number: TPS6594-Q1 Other Parts Discussed in Thread: SK-AM69 , , AM69 Hi,
We follow the SK-AM69 EVM to design the TPS6594-Q1, but can't bring up.
We have confirmed that the PMIC VINT and VRTC outputs are both at 1.8 V.
According to the specification…
Part Number: SK-AM69 Other Parts Discussed in Thread: AM69A , AM68 , AM69
Hi Expert,
Does the AM69A reference design/EVM require any mandatory firmware/programming before the system can boot (e.g., PMIC-related programming, boot configuration…
Part Number: SK-AM69 Tool/software: Based on my understanding, the sdk is built on ubuntu 22 while the same can not be installed onto the board directly. My question is if the kernel is modified, can we install Ubuntu 24 LTS? What potential issues could…
Part Number: SK-AM69 Tool/software: Hi All,
I have a moveit2 package in ros2 jazzy i need to deploy on this board. i was wondering what kind of performance history is available with moveit2. im guessing the operations will likely need to be headless…
Part Number: SK-AM69 Tool/software: Hello, We are evaluating your SK-AM69 platform. I am working with your Jacinto TDA4/DRA8 platform for a different project (just starting on this project). On the Jacinto, on the R Cores we run safeRTOS (freeRTOS) and…
Part Number: SK-AM69 Other Parts Discussed in Thread: AM69 Tool/software: The AM69 running Yocto Linux ( 10.01.00.05 (Dec 18, 2024) ) Is not able to enumerate large 64Bit prefetchable PCIe BARs on 3rd party endpoint hardware.
Is this a hardware limitation…
Part Number: SK-AM69
Tool/software:
Hi, I installed using ti-processor-sdk-linux-am69-sk-10_01_08_01-Linux-x86-Install.bin and flashed tisdk-default-image-am69-sk.rootfs.wic to the SD card.
I would like to use gst-launch-1.0 + RTSP + v4l2h264dec…
Part Number: SK-AM69
Tool/software:
Hi,
I'm working on project that requires memory allocation for DMA. While working on it, It seems like there is memory corruption on allocated memories.
So we made programs to test this.
dma_bridge.tar.gz…