Part Number: SK-AM69 Hi,
We need to use the PCIe in the SK-AM69 but the reference user guide is only the Edge AI that we can't search the PCIe configuration in below website,
and pleaes advise if there are any reference guide that we can test the P…
Part Number: SK-AM69 Other Parts Discussed in Thread: AM69 , TDA4VL , Tool/software: Can the R5F core in AM69 evaluation board be used to develop custom applications with free RTOS? the use casess are intercore communication with A72 and use display port…
Part Number: SK-AM69 From AM69-SK board. there are two type connectors for CSI.
Camera interfaces: three CSI-2 ports compatible with Raspberry Pi or a high-speed 40-pin Samtec camera connector allowing up to twelve cameras (requires multi camera hub) …
Part Number: SK-AM69 Other Parts Discussed in Thread: AM69 , AM69A
Hi TI experts,
On the SK-AM69 I try to control WKUP_GPIO0_28 for EN_EFUSE inside keywriter but unfortunately pin state on resistor R172 can't be set. For test purpose I block Sciclient_otpProcessKeyCfg…
Part Number: SK-AM69
Hi Experts,
I'm trying to work my TensorFlow Lite model using python3 and opencv. I'm planning to use a camera, but I'm trying from one image first.
Inference is no problem, but It cannot output the display using imshow…
Part Number: SK-AM69 Hi!
I inserted micro SD card in the slot and powerd ON the kit with 90W Dell charger. It is showing Edgi AI galley images. After closing the tab with top right 'X' it shows Evaluation kit photo with ip adress and PW. How to proceed…
Hi Brandon,
Brandon Brnich said: The cpu would have to be reading approximately 750 mega bytes per second per stream. You're getting into gigabytes when you have two streams. Two unique file sources is not feasible - it is too much raw data that has to…
Part Number: SK-AM69 Other Parts Discussed in Thread: MATHLIB Hello TI,
I am using a SK-AM69 Board and the SDK for j784s4 v9.2.0.5.
I boot Linux and program one of the C7120 DSP with a tiny test program using CCS 12.7.
The program calls MATHLIB_exp2…
HI Wayne
I generated the image based on the SDK 9.1 on top of that i applied the patch as mentioned in the reference thread
https://e2e.ti.com/support/processors-group/processors/f/processors-forum/1317252/sk-am69-wkup_gpio0-control-on-sk-am69/501576…
Part Number: SK-AM69 Other Parts Discussed in Thread: TDA4VM , , AM69 , TDA4VH
I was previously developing on the TDA4VM chip and there was a processor sdk rtos as well as a processor sdk linux
Now working with the SK-AM69 Demo board I do not see a processor…