Part Number: SK-TDA4VM Hi,
According to this guide https://software-dl.ti.com/jacinto7/esd/processor-sdk-linux-sk-tda4vm/09_01_00/exports/edgeai-docs/devices/TDA4VM/linux/getting_started.html#ov5640-yuv-sensor SK-TDA4VM Supports OV5640 YUV sensor camera…
Hello,
Apologies for the late reply. Is this thread still open? Either way, assuming the thread is open and others will benefit from this thread, I will post a response.
As a disclaimer, we do not recommend developing R5F and RTOS code on the SK-TDA4VM…
Part Number: SK-TDA4VM Other Parts Discussed in Thread: TDA4VM
Hi, Champ
we are developing board based on SK-TDA4VM, MMC connection is planned to change as follows for custom use.
MMCSD0 : eMMC flash (MTFC8GAMALBH-AAT) for BOOT/NOS. MMCSD1 : micro SD card…
Part Number: SK-TDA4VM Hi All,
As per last discussion, the proposed approach for the SK-TDA4VM QNX Academy demo doesn't work for us.
We have built the TI-PSDK QNX package for J721E EVM and tried to boot it in SK-TDA4VM board.
From the boot log, I…
Part Number: SK-TDA4VM Hi,
I am trying to make a code (.out) for the C71x processor in which I would like to communicate with the other processors. The project is located under the vision_apps/apps/utilities/my_program/...
When I try to build my project…
Hi Igor,
Igor Kovryga said: Does disabling CSI port No. 2 have an effect or is there another reason why the video stream does not arrive?
This shouldn't be an issue.
I would suggest you try using the yavta command once to stream and also check if the…
Part Number: SK-TDA4VM Hi,
Followiing is the board that we are using: https://www.ti.com/product/SK-TDA4VM/part-details/J721EXSKG01EVM
The reason of using this old SDK is to try out Jailhouse.
I have download the v7 SDK from the following link: https:/…
Part Number: SK-TDA4VM Hi,
We are currently using Yocto Linux 09.01 which comes with meta-qt5 layer. We wish to upgrade to meta-qt6 for running QT application which have been developed using QT6. We had replaced the meta-qt5 layer with meta-qt6 and updated…
Part Number: SK-TDA4VM
This is schematics of SK-TDA4VM which PEDET pin has no connection.
I wonder if SK-TDA4VM could select PCI-E or SATA for inserted device on M.2 M Key slot.
Can we select M KEY device to use PCI-e or SATA interface with Z-state on…
Part Number: SK-TDA4VM 1. Download ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05-Linux-x86-Install.bin and install. 2. execute sudo ti-processor-sdk-linux-adas-j721e-evm-09_02_00_05/bin/create-sdcard.sh, create SD rd with prebuilt Image in the sdk …