Part Number: SM320F28335-HT Hello,
I have a question regarding the 2.2uF caps that the data sheet says to add on the ADCREFx pins. What effect would using a 1uF cap on these pins have on the ADC readings/functionality, specifically when operating at 200…
Part Number: SM320F28335-HT Hello,
Could someone please clarify for me what voltage needs to be used for the VDD supply? The SM320F28335-HT datasheet calls for 1.9V, but the TMS320F2833F datasheet calls for 1.9V @ 150MHz and 1.8V @ 100MHz. I wanted to…
Sagar,
Both the "S" and "Q" suffix devices support Ta(free air) temps of 125C and Tj(junction) temps of 150C. The Q device also included Q100 qualification.
If you are looking for a device that support Ta = 150C(or higher) then you…
Part Number: SM320F28335-HT Hi There
i have an application where I need a processor to run for 20-30h hours at 230 degrees
can I run this part hotter than the datasheet value of 210 but for a reduced life?
Is there a cliff edge point where it stops working…
Hi Romero, TMS320F2837x got all the peripherals and computational power for motor control. we also have a variant TMS320F28377D-EP offering broader temperature range. Depending upon your motor control architecture, you may also want to consider TMS320F2800157…
Part Number: SM320F28335-HT Do you have any available SEU analysis available for SM320F28335, inparticular the configuration and control registers, is there difference from normal SRAM?
Thank you.
Ken Jewell.
Part Number: SM320F28335-HT Other Parts Discussed in Thread: C2000WARE Hi,
I'm porting a bootloader application to a SM320F28335-HT. I would like to use #pragma LOCATION as described in "TMS320C28x Optimizing C/C++ Compiler v18.12.0.LTS"/spru514r.pdf…
Part Number: SM320F28335-HT Hi There
Section 3.6.1.1 (external reference oscillator clock option) says its not guaranteed above 125 degrees. My assumption is this note is referring to a "external" crystal for use with the "internal" on chip oscillator…
Part Number: SM320F28335-HT Other Parts Discussed in Thread: CONTROLSUITE , C2000WARE-MOTORCONTROL-SDK Tool/software: Code Composer Studio I note there no high temp newer C2000 MCU that replace F28835. Most newer MCU with improved motor supports are all…
Part Number: SM320F28335-HT Hello,
We need the die format of the SM320F28335.
According to TI and Digikey, the part number is
SM320F28335 KGDS1
But looking at stock at Micross, they only have the
SM320F28335 SKBD1
What is the difference? Are dice in Micross…