Part Number: SMARTRF06EBK Other Parts Discussed in Thread: CC2642R , ENERGYTRACE Hello,
I am using SMARTRF06EBK to flash firmware via cJTAG onto our device that operates on CC2642 MCU. I am designing a custom device for a more convenient flashing procedure…
Part Number: SMARTRF06EBK Ran into "Failed to load the CPU core driver" message when starting the IAR 8.32.2 debugger using the SmartF06 emulator (TI XDS).
I have re-installed the ti_emupack_setup_9.2.0.00002_win_64.exe also and didn't help.
Below…
Part Number: SMARTRF06EBK Other Parts Discussed in Thread: CC2650 Hi Team,
Can you please check and advise with following request?
"
I have a SmartRF06EB and CC2650. I could not find how to read the acceleration values from the BMA250E accelerometer…
Part Number: SMARTRF06EBK We wish to connect an analog input device, e.g., a microphone, to the EB06 and should like to know if anyone has had any experience or could refer to a reference?
Regards
Ron Barker
Part Number: SMARTRF06EBK Other Parts Discussed in Thread: CC2640R2F Tool/software: TI C/C++ Compiler I'm working with both boards and need to use the I2C interface, for the LAUNCHXL there's enough information for the pin map (concise and precise): DIO4…
Part Number: SMARTRF06EBK Other Parts Discussed in Thread: CC2538 Hi All,
Is the default setting for the SMARTRF06EBK device to remain on one channel and is there a methode to have channel hopping with this tool?
- Leo
Part Number: CC2640 Other Parts Discussed in Thread: SMARTRF06EBK ,
Dear Experts,
I am using the following BTool (v1.40.5).
Does this BTool (v1.40.5) work well on Windows 10 (64bit)?
If Windows 10 (64bit version) is released, could you please…
Thank you for the information
i need to store the temperature sensor data in sdcard at the coordinator board(smartrf06 baord attached with cc2538em) what are the APIs functions to be used to store the data in sdcard