Part Number: SN3257-Q1 Tool/software: Hi,
Can someone please confirm if the above mentioned mux can be used for UART signals as I didn't find anything on usage for UART signals in datasheet.
Part Number: SN3257-Q1 Tool/software: Hello Application team:
We would like use SN3257-Q1 design for standard I2C 2:1 switch control as like application.
Could you please help review the design can workable for Standard I2C(100k /400k) switch selection…
Part Number: SN3257-Q1 Tool/software: Dears,
My customer uses SN3257 for power-off protection, but there is leakage of 0.3V, which makes it impossible to achieve complete isolation. Is there any solution?
Many thanks!
Arabella Zhang
Part Number: SN3257-Q1 Tool/software: Hi ,
I've downloaded IBIS model from your website for this analog switch, but it doesn't work after I imported it into the sim tool. No matter how I tune the SEL/EN, and add some voltage levels at the pin a1 and…
Part Number: SN3257-Q1 Tool/software: Hello,
I am trying to use the SN3257-Q1 IBIS model in Sigrity. I wounder if anyone has run this in Sigrity.
The reason I am asking is because I am having issues to run the simulation because it asks for selecting…
Part Number: SN3257-Q1 Hello,
I'm using this component to connect two different SPI devices (Device A on SxA pins and Device B on SxB pins) to one SPI net (on Dx pins).
Device B can be phisically disconnected from the switch.
Question: are needed…
Part Number: SN3257-Q1 Hi BU team
Is SN3257-Q1 ok for RGMII switch function? If it is not ok, would you help promote the right part ? This is an automotive application and need Q-grade device.
Thanks
Part Number: SN3257-Q1 Tool/software: Hi team,
We use SN3257, and found in the experiment that the two pins S1B and S3B are short-circuited to the ground. My SA and SB are connected to two MCUs at the same time, and both MCUs fail at the same time.…