Part Number: SN54LVCH245A-SP Tool/software: Hello,
we are employing the SN54LVCH245A-SP as input / output buffer for an aerospace application.
There's some requirement about output rise / fall time, unfortunately these parameters are not specified…
Part Number: SN54LVCH245A Other Parts Discussed in Thread: SN74LVCH245A Hi,
There is a thermal pad on the underside of the device, but there is no any description of which signal the thermal pad should connect to.
Can I connect the thermal pad connect…
Part Number: SN54LVCH245A-SP The website states the SNJ54LVCH245-SP is radiation tolerant but I can’t find any details or test data. Do you have any information on this parts radiation capability?
Other Parts Discussed in Thread: SN54LVCH245A Hi All,
I hope all is well. I am running SI analysis on one of our existing board that utilizes the follow interface: SNJ54LVCH245AJ, SNJ55LVDS31J. Could you please support with the provision of its IBIS…
Hi Wade,
Thanks a lot for the clarifications.
These parts are not visible on TI website so i was not able to confirm if they are TI or not.
I will create a separate thread for each of the components below:
5962-9762101QEA SN55LVDS31 5962-9754301QEA…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…