Part Number: SN54LVTH16244A We attempted to solder Ti driver (SN54LVTH16244A Ti) on submount with AuSn solder. The processing temperature is 330 degree C for 1.5 minutes. After soldering, we notice shorts between pads. Are those shorts associated with…
Part Number: SN54LVTH16244A Team,
Can you share information about the internal ESD protection on the SN54LVTH16244A?
I need to design a protection circuit that interfaces with this buffer against a 4kV ESD transient following the Human Body Model…
Part Number: SN54LVTH16244A-SP Hi,
I can not find the Radiation & Reliability reports of the componet SN54LVTH16244A-SP.
Could you please point me the link?
Thanks a lot.
cheers.
Other Parts Discussed in Thread: SN54LVTH16244A Team,
Can you please help with the following issue:
Can you provide any details on the operation and type of bus hold circuit implemented on the SN54LVTH16244A inputs?
We’re seeing odd behavior of…
Ankita, We do not have IBIS models for these two devices. However, we do have IBIS models for both in the A versions with WD parasitics. For SN54LVTH16244A : www.ti.com/.../slym084 For the SN54LVTH16245A : www.ti.com/.../slym083 Note, both of these are…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…