Part Number: SN54LVTH244A-SP Could you let me know the package information as follows?
P/N: 5962-9584401VSA
・Package material/ base plating /plating (ex. Ceramic(Alumina)/Ni/Au
・Lid material/ base plating /plating (ex. Covar/Ni/Au
・Package cavity…
Part Number: SN54LVTH244A-SP Other Parts Discussed in Thread: SN54LVTH244A , SN74LVTH244A Hi Sir/Mdm,
The datasheet for SN54LVTH244A does not indicate any value for IOFF. Is it because it is not tested or there is no such parameter?
Similar part …
Part Number: SN54LVTH244A-SP Team,
Quick question from my customer:
The data sheet for the 54LVTH244A has the following requirements under recommended operation for power supply rise time:
What is the impact to part functionality if the power…
Part Number: SN54LVTH244A-SP abs max rating lists "current into any output in the high state, Io" only for Vo > Vcc (Note 2). Is there abs max rating for high state current when Vo < Vcc?
Part Number: SN54ACT244 Other Parts Discussed in Thread: SN54LVCH244A , SN54LVTH244A Dear Design support team.
It is designed as below.
The redundant IC is in not-supplied. (The primary and redundant channel will be changed in specific condition…
An isolator like the ISO7041-Q1 makes sense only for galvanic isolation.
The SN3257-Q1 would be able to disconnect the signals. Alternatively, use any buffer with Ioff protection, e.g., SN74LV125A-Q1 or SN54LVTH244A-SP.
Other Parts Discussed in Thread: SN54LVCH244A , SN54LVC541A , SN54LVTH244A Hello,
We have read through the SNJ54AC244W datasheet and this document on CMOS devices http://www.ti.com/lit/an/scba004c/scba004c.pdf , but I'm having trouble finding the following…
Hi Jenny,
As far as I know, TPSM846C24 module is not specifically manufactured to withstand radiation.
You may find some SEE TI products here: e2e.ti.com/.../slyt532g.pdf
Martin,
As I mentioned previously, we do not have such information. Our Modules are for commercial use therefore those tests are not performed.
I would recommend going to ti.com, click on top left corner "Applications" and select "Aerospace & defense…